SPRUJD0 July 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The use case page is shown in Figure 3-1. This sheet has 10 different sections that must be completed.
This block allows the user to assign a utilization to each major core IP.
This block allows the user to select the frequency for the key blocks in the core utilization block (+DDR).
The AM67x device has a Double Data Rate (DDR) SDRAM controllers and associated physical layer interfaces (PHYs) as well as a General-Purpose Memory Controller (GPMC) with Error Location Module (ELM).
The AM67x device has several PHYs; for the PHYs with multiple instances, in addition to the mode and the utilization, the user should also select how many of the instances are used:
There are two high speed serializing / deserializing (SerDes) interfaces on this device. Each SerDes has a single lane for which the mode, utilization, and IP should be selected.
The tool cannot determine the loading of the IP from the SerDes loading. Therefore, it is required that the user enter the IP loading in this table as well as entering the SerDes loading.
The environmental section allows the user to define junction temperature (Tj), VDD_CPU_AVS voltage, VDD_MCU voltage, the process corner, and a use case name and description.
Like the PHY section, the user enters Mode, utilization, and instances for each LVCMOS.
There is only one mode and utilization allowed per IP (customization is not supported since the corresponding IP blocks do not contribute significantly to the overall power). If a system uses multiple modes for an IP type, the highest power mode should be used.
The buttons initialize different phases of the power estimation.
When each button is pushed, the cells underneath the button (H8:I11) record that it was started and then record when the step completes.
This drop down selects the use case to pre-populate.
This set of use cases is supplemented when the user saves the current UC (with the buttons described above).
The pre-populated use cases are intended to provide TI-generated starting points for the customer’s use case. In the final section of this user guide, some of the pre-populated use cases will be discussed.