SPRUJD8 June 2024 TDA4APE-Q1 , TDA4VPE-Q1
The EVM supports one USB3.1 Gen1 Type C interface [J4], which can function as DFP, UFP, or DRP. The configurable modes provide support for the USB boot modes of the processor. For details on how to select the USB mode, see Section 2.4.2. The VBUS output for this port is limited to 1.5A. When operating as UFP, the EVM cannot be powered from this port.
The EVM also supports two USB2.0 Type A interfaces [J5] via an on-board USB hub. These ports can only function as Host. The VBUS output for each port is limited to 0.5A.
The processor supports a single USB interface. Therefore, the user must configure for either the USB3.1 Type C interface or the USB2.0 Type A interface. Both cannot be operated simultaneously