SPRUJD8 June 2024 TDA4APE-Q1 , TDA4VPE-Q1
The EVM provides several expansion interfaces that have non-standard/custom pinouts. Each of these interfaces are introduced and specific pin information is provided.
Note that some of the interfaces include ‘Direction’ information. This is relative to the EVM, so INPUT is input to the EVM/output of the connected device. OUTPUT is output of the EVM/input to the connected device.