SPRUJD8 June 2024 TDA4APE-Q1 , TDA4VPE-Q1
The EVM supports a manual switch [SW1] for power control to the EVM. The switch [SW1] is a two-position switch. The OFF position disconnects input power from on-board circuitry. The ON position connects the input power.
Three status LEDs [LD7][LD8][LD9] are used to communicated power status to the user.
LED | ‘ON’ State | ‘OFF’ State |
---|---|---|
[LD7] | Power switch [SW1] is in the ON position, and input power is being supplied to the EVM. | Power switch [SW1] is in the OFF or there is some other issue causing power to not be supplied. |
[LD8] | MCU domain of the EVM is powered | MCU domain of the EVM is not powered/OFF (1) |
[LD9] | MAIN domain of the EVM is powered | MAIN domain of the EVM is not powered/OFF (1) |