SPRUJE1 July 2024
The XDS110 board includes an emulation header and High-density connector to interface with the controlSOM. The XDS110 board includes the circuitry needed for XDS110 emulation.
The unidirectional pins of the ISO1644 digital isolator are used to isolate the JTAG signals of the XDS110 circuit from the isolated emulator connector. For implementation of cJTAG mode, the TMS signal is also routed through a slower, bidirectional input on a second ISO1644. A switch (S1) is used to select between JTAG and cJTAG mode.