SPRUJF4A October 2024 – December 2024
As explained in Section 2.1.5, there is a comparator U10 for external overcurrent protection. Figure 4-19 shows the eternal overcurrent protection waveform. Output (net IPM_CIN) of U10 is high when current on R80 exceeds the reference point set by negative input of U10, high-level IPM_CIN then triggers IPM fault protect to output a low-level signal at IPM_FAULT, which is connected to the microcontroller.