SPRUJG2 December 2024 AM62D-Q1
The boot mode for the EVM board is defined by two banks of switches SW1 and SW2. This allows for AM62D SoC Boot mode control by either the user (DIP Switch Control).
All the bits of switch (SW1 and SW2) have a weak pull down resistor and a strong pull up resistor as shown in Figure 2-3. Note that OFF setting provides a low logic level (‘0’) and an ON setting provide a high logic level (‘1’).
The boot mode pins of the SoC have associated alternate functions during normal operation. Hence isolation is provided using Buffer ICs to cater for alternate pin functionality. The output of the buffer is connected to the boot mode pins on the AM62D SoC and the output is enabled only when the boot mode is needed during a reset cycle.
The input to the buffer is connected to the DIP switch circuit and to the output of an I2C I/O Expander set by the test automation circuit. If the test automation circuit controls the boot mode, all the switches should be manually set to the OFF position. The boot mode buffer is powered by an always ON power supply to ensure that the boot mode remains present even if the SoC is power cycled.
Switch SW1 and SW2 bits [15:0] are used to set the SoC boot mode.
The switch map to the boot mode functions is provided in the following tables.
Bit15 | Bit14 | Bit13 | Bit12 | Bit11 | Bit10 | Bit9 | Bit8 | Bit7 | Bit6 | Bit5 | Bit4 | Bit3 | Bit2 | Bit1 | Bit0 |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Reserved | Reserved | Backup Boot Mode Configuration | Backup Boot Mode | Primary Boot Mode Configuration | Primary Boot Mode | PLL Configuration |
SW2.3 | SW2.2 | SW2.1 | PLL REF CLK (MHz) |
---|---|---|---|
OFF | OFF | OFF | 19.2 |
OFF | OFF | ON | 20 |
OFF | ON | OFF | 24 |
OFF | ON | ON | 25 |
ON | OFF | OFF | 26 |
ON | OFF | ON | 27 |
ON | ON | OFF | RSVD |
ON | ON | ON | RSVD |
SW2.7 | SW2.6 | SW2.5 | SW2.4 | Primary Boot Device Selected |
---|---|---|---|---|
OFF | OFF | OFF | OFF | Serial NAND |
OFF | OFF | OFF | ON | OSPI |
OFF | OFF | ON | OFF | QSPI |
OFF | OFF | ON | ON | SPI |
OFF | ON | OFF | OFF | Ethernet RGMII |
OFF | ON | OFF | ON | Ethernet RMII |
OFF | ON | ON | OFF | I2C |
OFF | ON | ON | ON | UART |
ON | OFF | OFF | OFF | MMC/SD card |
ON | OFF | OFF | ON | eMMC |
ON | OFF | ON | OFF | USB0 |
ON | OFF | ON | ON | GPMC NAND |
ON | ON | OFF | OFF | GPMC NOR |
ON | ON | OFF | ON | Rsvd |
ON | ON | ON | OFF | xSPI |
ON | ON | ON | ON | No boot/Dev Boot |
SW1.2 | SW1.1 | SW2.8 | Boot Device |
---|---|---|---|
Reserved | Read Mode 2 | Read Mode 1 | Serial NAND |
Reserved | Iclk | Csel | QSPI |
Reserved | Iclk | Csel | OSPI |
Reserved | Mode | Csel | SPI |
Clkout | 0 | Link Info | Ethernet RGMII |
Clkout | Clk src | 0 | Ethernet RMII |
Bus Reset | Reserved | Addr | I2C |
Reserved | Reserved | Reserved | UART |
1 | Reserved | Fs/raw | MMC/ SD card |
Reserved | Reserved | Reserved | eMMC |
Core Volt | Mode | Lane swap | USB0 |
Reserved | Reserved | Reserved | GPMC NAND |
Reserved | Reserved | Reserved | GPMC NOR |
Reserved | Reserved | Reserved | Reserved |
SFPD | Read Cmd | Mode | xSPI |
Reserved | ARM/Thumb | No/Dev | No boot/Dev Boot |
SW1.5 | SW1.4 | SW1.3 | Backup Boot Device Selected |
---|---|---|---|
OFF | OFF | OFF | None(No backup mode) |
OFF | OFF | ON | USB |
OFF | ON | OFF | Reserved |
OFF | ON | ON | UART |
ON | OFF | OFF | Ethernet |
ON | OFF | ON | MMC/SD |
ON | ON | OFF | SPI |
ON | ON | ON | I2C |