SPRZ171T December 2004 – September 2020 SM320F2801-EP , SM320F2808-EP , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F2806 , TMS320F2806-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2809-Q1
This document describes the silicon updates to the functional specifications for the TMS320F2809, TMS320F2808, TMS320F2806, TMS320F2802, TMS320F2801, TMS320C2802, TMS320C2801, TMS320F28016, and TMS320F28015 digital signal processors (DSPs).
The updates are applicable to:
Throughout this document, the device names are abbreviated as follows:
Throughout this document, any reference to F2801 and F2802 devices includes both 60-MHz and 100-MHz versions.
To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of all [TMS320] DSP devices and support tools. Each TMS320™ DSP commercial family member has one of three prefixes: TMX, TMP, or TMS (for example, TMS320F2808). Texas Instruments recommends two of three possible prefix designators for its support tools: TMDX and TMDS. These prefixes represent evolutionary stages of product development from engineering prototypes (TMX/TMDX) through fully qualified production devices/tools (TMS/TMDS).
TMX | Experimental device that is not necessarily representative of the final device's electrical specifications | |
TMP | Final silicon die that conforms to the device's electrical specifications but has not completed quality and reliability verification | |
TMS | Fully qualified production device |
Support tool development evolutionary flow:
TMDX | Development-support product that has not yet completed Texas Instruments internal qualification testing | |
TMDS | Fully qualified development-support product |
TMX and TMP devices and TMDX
development-support tools are shipped against the following disclaimer:
"Developmental product is intended for internal
evaluation purposes."
TMS devices and TMDS development-support tools have been characterized fully, and the quality and reliability of the device have been demonstrated fully. TI's standard warranty applies.
Predictions show that prototype devices (TMX or TMP) have a greater failure rate than the standard production devices. Texas Instruments recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.
TI device nomenclature also includes a suffix with the device family name. This suffix indicates the package type (for example, GBA) and temperature range (for example, A).
Figure 3-1 provides an example of the TMS320F280x device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 3-1. Some prototype devices may have markings different from those illustrated. Figure 3-2 shows an example of device nomenclature.
SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | F2809 COMMENTS |
---|---|---|---|
Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMS. |
A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | C2801, C2802 COMMENTS |
---|---|---|---|
Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX only. |
A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | F2801, F2802, F2806, and F2808 COMMENTS | F28015 and F28016 COMMENTS |
---|---|---|---|---|
Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX only. | TI internal only |
A | Indicates Revision A | 0x0001 | This silicon revision is available as TMX only. | TI internal only |
B | Indicates Revision B | 0x0002 | This silicon revision is available as TMS. | TI internal only |
C | Indicates Revision C | 0x0003 | This silicon revision is available as TMS. | This silicon revision is available as TMS. |
Table 4-1 to Table 4-3 list the change(s) made to each silicon revision.
REVISION | CHANGES MADE |
---|---|
A | The following advisory was fixed: "Input Clock: Device Startup Using XCLKIN Input". |
0 | First silicon release. (This is functionally equivalent to Revision C of the TMS320F280x silicon.) |
REVISION | CHANGES MADE |
---|---|
A | TMS silicon (This is functionally equivalent to Revision C of the TMS320F280x silicon.) |
0 | First silicon release. (This is functionally equivalent to Revision B of the TMS320F280x silicon - TI Internal only) |
REVISION | CHANGES MADE |
---|---|
C | The following advisories were fixed:
|
B |
|
A | The following advisories were fixed:
|
0 | First silicon release. |