SPRZ171T December 2004 – September 2020 SM320F2801-EP , SM320F2808-EP , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F2806 , TMS320F2806-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2809-Q1
SCI: Incorrect Operation of SCI in Address Bit Mode
0, A on F2809 silicon
0, A on C280x silicon
0, A, B, C on F2801, F2802, F2806, F2808, and F2801x silicon
SCI does not look for STOP bit after the ADDR bit. Instead, SCI starts looking for the start bit beginning on sub-sample 6 of the ADDR bit. Slow rise-time from ADDR to STOP bit can cause the false START bit to occur since the 4th sub-sample for the start bit may be sensed low.
Program the baud rate of the SCI to be slightly slower than the actual. This will cause the 4th sub-sample of the false START bit to be delayed in time, and therefore occur more towards the middle of the STOP bit (away from the signal transition region). The amount of baud slowing needed depends on the rise-time of the signal in the system. Alternatively, IDLE mode of the SCI module may be used, if applicable.