SPRZ408D June   2014  – June 2021 AM4372 , AM4376 , AM4377 , AM4378 , AM4379

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Device and Development Support Tool Nomenclature
    2. 1.2 Revision Identification
  3. 2All Errata Listed With Silicon Revision Number
  4. 3Usage Notes and Known Design Exceptions to Functional Specifications
    1. 3.1 Usage Notes
      1. 3.1.1 LPDDR2/DDR3: JEDEC Compliance for Minimum Self-Refresh Command Interval
      2. 3.1.2 DDR3/DDR3L: JEDEC Specification Violation for DDR3 RESET Signal When Implementing RTC+DDR Mode
    2. 3.2 Known Design Exceptions to Functional Specifications
      1. 3.2.1 Advisory List
      2.      Advisory 1
      3.      Advisory 2
      4.      Advisory 3
      5.      Advisory 4
      6.      Advisory 5
      7.      Advisory 6
      8.      Advisory 7
      9.      Advisory 8
      10.      Advisory 9
      11.      Advisory 10
      12.      Advisory 11
      13.      Advisory 12
      14.      Advisory 13
      15.      Advisory 14
      16.      Advisory 15
      17.      Advisory 16
      18.      Advisory 17
      19.      Advisory 19
      20.      Advisory 20
      21.      Advisory 21
      22.      Advisory 22
      23.      Advisory 24
      24.      Advisory 25
      25.      Advisory 26
      26.      Advisory 27
      27.      Advisory 28
      28.      i2223
      29.      i2224
      30.      i912
      31.      i2225
      32.      i2226
  5. 4Revision History

Revision Identification

The device revision can be determined by the symbols marked on the top of the package. Figure 1-1 provides an example of the device markings.

GUID-ECE09E29-8D51-44B8-9E75-A23AF2F12EFC-low.gif Figure 1-1 Example of Device Revision Codes for the Device Processor

NOTES:

  1. Non-qualified devices are marked with the letters "X" or "P" at the beginning of the device name, while qualified devices have a "blank" at the beginning of the device name.
  2. The device shown in this device marking example are two of several valid part numbers for the family of devices.
  3. The device revision code is the device revision (A, B, and so on).
  4. YM denotes year and month.
  5. LLLL denotes Lot Trace Code.
  6. 631 is a generic family marking ID.
  7. G1 denotes green, lead-free.
  8. ZDN is the package designator.
  9. S denotes Assembly Site Code.
  10. On some "X" devices, the device speed may not be shown.

Silicon revision is identified by a code marked on the package. The code is of the format AM4376x, where "x" denotes the silicon revision. Table 1-1 lists the information associated with each silicon revision for each device type. For more details on device nomenclature, see the device-specific data manual.

Table 1-1 Production Device Revision Codes
DEVICE REVISION CODESILICON REVISIONCOMMENTS
A1.1Silicon revision PG1.1
B1.2Silicon revision PG1.2

Each silicon revision uses a specific revision of TI's ARM® Cortex®-A9 processor. The ARM Cortex-A9 processor variant and revision can be read from the Main ID Register. The DEVREV field (bits 31-28) of the Device_ID register located at address 0x44E10600 provides a 4-bit binary value that represents the device revision. The ROM code revision can be read from address 0x3BFFC on silicon revision 1.1 and 0x3FFFC on silicon revision 1.2. The ROM code version consists of two decimal numbers: major and minor. The major number is 0x27, and the minor number counts ROM code version. The ROM code version is coded as hexadecimal readable values; for example, ROM version 27.02 is coded as 0x2702. Table 1-2 shows the ARM Cortex-A9 Variant and Revision, Device Revision, and ROM Code Revision values for each silicon revision of the device.

Table 1-2 Silicon Revision Variables
SILICON
REVISION
ARM CORTEX-A9
VARIANT AND REVISION
DEVICE
REVISION
ROM
REVISION
PL310 CACHE CONTROLLER VERSION
1.1r2p100001b27.01r3p2
1.2r2p100002b27.02r3p2