SDFM: Manchester Mode (Mode 2) Does Not Produce Correct Filter Results Under Several
Conditions
Revisions Affected
0,
A, B, C
Details
The Manchester decoding algorithm
samples the Manchester bitstream with SYSCLK in a calibration window of 1024 SDx_Dy
signal transitions. The derived clock from the Manchester bitstream is used to
sample for data in the subsequent calibration window cycle.
There are several scenarios that can
cause large errors in the filter results:
- Any single noise event on
SDx_Dy can corrupt the decoded Manchester clock and cause subsequent data to
be sampled at an incorrect frequency.
- If the Manchester bitstream
clock rate is a near exact integer multiple of SYSCLK, then an occasional
Manchester bit can be skipped when the phases of the Manchester stream and
internal SYSCLK drift past each other in phase before the next 1024
transition calibration window becomes effective. Deviations in duty cycle
from 50% of the Manchester clock also need to be accounted for to ensure the
longer Manchester pulses are not an integer multiple of SYSCLK. This
situation can be unavoidable if the clock sources for either the SD
modulator or this device have a wide variation since a wide range of keep
out frequencies become problematic
- If the Manchester edge delay
variation between rising and falling (duty cycle of the bitstream) is
greater than one SYSCLK, then the SDFM clock decode algorithm can
incorrectly identify the clock period as shorter than it is.
Workarounds
The workarounds available are:
- Avoid using Manchester mode
and consider using Mode 0, which provides the best filter performance under
noisy conditions. This is the recommended workaround.
- Avoid any noise on the
Manchester bitstream and avoid integer multiples of SYSCLK for the selected
Manchester clock source. A precision clock source for the modulator and this
device must be used.
- Ensure rising and falling
edge delays (high and low pulses) are within one SYSCLK of each other in
length.
- Design an application-level
algorithm that is robust against occasional incorrect SDFM results.