SPRZ452I july 2018 – may 2023 AM6526 , AM6528 , AM6546 , AM6548
CSI: Interface Setup/Hold Timing Does Not Meet MIPI DPHY Spec above 600MHz
When running the CSI2 interface at greater than 600MHz (1.2Gbps per lane), setup/hold times are not compliant with limits required by the MIPI CSI2 DPHY specification. Systems using the CSI2 interface at less than or equal to 600MHz are not affected.
Since the CSI2 interface includes up to 4 data lanes (plus 1 clock lane), data can be distributed across multiple lanes in order to keep the clock rate lower.