SPRZ452I july 2018 – may 2023 AM6526 , AM6528 , AM6546 , AM6548
CPSW: CPSW Directed Frames are Not Observed When
Classification Overrides the Destination Port Via the Egress Opcode Feature
Directed frames sent via software with the 802.1CB header are incorrectly redirected back to the host port. Directed frames should not be overridden by the ALE Egress Op logic.
Ensure that the Host traffic is excluded from the classifier.