SPRZ452I july 2018 – may 2023 AM6526 , AM6528 , AM6546 , AM6548
On-Chip Debug: CPTracer Bus Probes MAIN_CAL0_0 and MCU_SRAM_SLV_1 are not able to Distinguish between Secure and Non-secure Transactions
AM65x SR 2.1, SR 2.0, SR 1.0
The CPTracer Bus Probe supports filtering on the properties of bus transactions including a property 'psecure' that identifies a transaction as being secure or non-secure. In the case of bus probe instances supporting MAIN_CAL0_0 and MCU_SRAM_SLV_1, the 'psecure' property will always indicate that a transaction is non-secure even if it were actually secure.
There are no workarounds for this issue. The user needs to be aware that secure and non-secure transactions are not distinguishable for MAIN_CAL0_0 and MCU_SRAM_SLV_1 CPTracer Bus Probes.