SPRZ457I January   2021  – December 2024 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2287
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2103
      4.      i2184
      5.      i2189
      6.      i2236
      7.      i2185
      8.      i2196
      9.      i2207
      10.      i2208
      11.      i2228
      12.      i2232
      13.      i2244
      14.      i2245
      15.      i2091
      16.      i2235
      17.      i2303
      18.      i2317
      19.      i2134
      20.      i2257
      21.      i2277
      22.      i2285
      23.      i2310
      24.      i2311
      25.      i2313
      26.      i2328
      27.      i2241
      28.      i2279
      29.      i2307
      30.      i2320
      31.      i2329
      32.      i2331
      33.      i2243
      34.      i2249
      35.      i2256
      36.      i2274
      37.      i2278
      38.      i2306
      39.      i2363
      40.      i2312
      41.      i2371
      42.      i2366
      43.      i2138
      44.      i2253
      45.      i2259
      46.      i2283
      47.      i2305
      48.      i2326
      49.      i2368
      50.      i2383
      51.      i2401
      52.      i2409
      53.      i2291
      54.      i2413
      55.      i2414
      56.      i2415
      57.      i2417
      58.      i2418
      59.      i2419
      60.      i2420
      61.      i2422
      62.      i2423
      63.      i2431
      64.      i2433
      65.      i2434
      66.      i2435
  4.   Trademarks
  5.   Revision History

Usage Notes and Advisories Matrices

Table 2-3 lists all usage notes and the applicable silicon revision(s). Table 1-2 lists all advisories, modules affected, and the applicable silicon revision(s).

Table 1-1 Usage Notes Matrix
ID DESCRIPTION SILICON REVISIONS AFFECTED
AM64x/AM243x 1.0 AM64x/AM243x 2.0
Package i2287 — Package Pin Assignment Difference between SR1.0 and SR2.0 YES YES
OSPI i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash YES YES
PLL i2424 — PLL: PLL Programming Sequence May Introduce PLL Instability YES YES
Table 1-2 Advisories Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM64x/AM243x 1.0 AM64x/AM243x 2.0
BCDMA i2431 — BCDMA: RX Channel can lockup in certain scenarios YES YES
Boot i2328 — Boot: USB MSC boots intermittently YES YES
Boot i2257 — xSPI boot mode redundant image boot failure YES NO
Boot i2307 — Boot: ROM does not properly select OSPI clocking modes based on BOOTMODE YES YES
Boot i2306 — Boot: ROM does not turn off internal termination resistors in SERDES YES NO
Boot i2363 — Boot: Peak voltage transitions may exceed PCIe spec during PCIe boot YES YES
Boot i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation YES YES
Boot i2371 — Boot: ROM code may hang in UART boot mode during data transfer YES YES
Boot i2413 — Boot: HS-FS ROM boots corrupted ROM boot image YES YES
Boot i2414 — Boot: Ethernet PHY Scan and Bring-Up Flow doesn't work with PHYs that don't support Auto Negotiation YES YES
Boot i2415 — Boot: UART Backup Boot Authentication Failure w/ xSPI Primary Boot Mode YES YES
Boot i2417 — Boot: GPMC NAND configured to slower clock speed YES YES
Boot i2418 — Boot: Secure ROM Panic due to Certificate Info not present YES YES
Boot i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled YES YES
Boot i2420 — Boot: XSPI Boot time is not consistent in SFDP mode YES YES
Boot i2422 — Boot: ROM timeout for MMCSD filesystem boot too long YES YES
Boot i2423 — Boot: HS-FS ROM applies debug access restrictions to all address space covered by the efuse controller firewall YES YES
Boot i2435 — Boot: ROM timeout for eMMC boot too long YES YES
CBASS i2207 — CBASS: Command Arbitration Blocking YES YES
CBASS i2235 — CBASS Null Error Interrupt Not Masked By Enable Register YES YES
CPSW i2184 — CPSW: IET express traffic policing issue YES YES
CPSW i2185 — CPSW: Policer color marking issue YES YES
CPSW i2208 — CPSW: ALE IET Express Packet Drops YES YES
CPSW i2331 — CPSW: Device lockup when reading CPSW registers YES YES
CPSW i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES YES
DebugSS i2317 — Debug is not available after TRST pin de-assertion when device pin EMU1 is repurposed as MCU_OBSCLK0 YES NO
DEBUG i2283 — Restrictions on how CP Tracer Debug Probes can be used YES YES
DEBUG i2291 — Debug: ATB Hang during Cortex-A53 trace YES YES
DDR i2232 — DDR: Controller postpones more than allowed refreshes after frequency change YES YES
DDR i2244 — DDR: Valid stop value must be defined for write DQ VREF training YES YES
DDR i2259 — DDR: Possibility of starvation of low priority commands YES YES
DDR i2274 — DDR: Including DDR in BSCAN causes current alarm on the DDR supply YES NO
DMA i2285 — BCDMA: Blockcopy Gets Corrupted if TR Read Responses Interleave with Source Data Fetch YES NO
DMA i2320 — BCDMA and PKTDMA: Descriptors and TRs required to be returned unfragmented YES NO
DMSC i2245 — DMSC: Firewall Region requires specific configuration YES YES
ECC_AGGR i2049 — ECC_AGGR: Potential IP Clockstop/Reset Sequence Hang due to Pending ECC Aggregator Interrupts YES YES
GPMC i2313 — GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO YES NO
Internal Diagnostic Modules i2103 — Incorrect Reporting of ECC_GRP, ECC_BIT and ECC_TYPE Information for Functional Safety Errors YES YES
Interrupt Aggregator i2196 — IA: Potential deadlock scenarios in IA YES YES
ICSSG i2305 — ICSSG: PRU RAM WRT during active FDB lookup write data corruption YES YES
ICSSG i2368 — ICSSG: Device lockup when reading registers in ICSSG module YES YES
ICSS i2433 — ICSS: Reading the 64-bit IEP timer does not have a lock MSW logic when LSW is read YES YES
ICSS i2434 — ICSS: IEP RX SOF and TX SOF capture register issue in 32-bit shadow mode when nano seconds part is zero YES YES
JTAG i2228 — JTAG: TAP used by Debuggers may be inaccessible if TRSTn device pin is never asserted YES NO
MCAN i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID YES YES
MCAN i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID YES YES
MDIO i2329 — MDIO: MDIO interface corruption (CPSW and PRU-ICSS) YES YES
MMCSD i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small YES YES
OSPI i2189 — OSPI: Controller PHY Tuning Algorithm YES YES
OSPI i2303 — OSPI: OSPI0_LBCLK0 pin has input floating by default YES NO
OSPI i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable YES YES
OSPI i2383 — OSPI: 2-byte address is not supported in PHY DDR mode YES YES
PCIe i2236 — PCIe: SERDES output reference clock cannot be used YES NO
PCIe i2241 — PCIe: The SerDes PCIe Reference Clock Output can exceed the 5.0 GT/s Data Rate RMS jitter limit YES NO
PCIe i2256 — PCIe: MSI or MSI-X does not trigger interrupt if address is not aligned to 8-bytes YES NO
PCIe i2243 — PCIe: Timing requirement for disabling output refclk during L1.2 substate is not met YES YES
PCIe i2326 — PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits YES YES
POK i2277 — POK: De-Glitch (filter) is based upon only two samples YES NO
PRG i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure YES YES
PSIL i2138 — PSIL: Configuration accesses and source thread teardowns may cause data corruption YES YES
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set YES YES
USART i2310 — USART: Erroneous clear/trigger of timeout interrupt YES YES
USART i2311 — USART: Spurious DMA Interrupts YES YES
USB i2091 — USB: USB 2.0 PHY hangs if received signal amplitude crosses squelch threshold multiple times within the same packet YES NO
USB i2134 — USB: USB 2.0 Compliance Receive Sensitivity Test Limitation YES NO
USB i2409 — USB: USB2 PHY locks up due to short suspend YES YES