SPRZ491D december 2020 – june 2023 DRA821U , DRA821U-Q1
CBASS: Command Arbitration Blocking
When the interconnect arbitrates commands from multiple sources, the higher priority request always takes precedence. Requests that are at the same priority level are arbitrated in round-robin fashion. The issue is after the higher priority request goes idle and there are two or more pending requests that are at the same priority level, the hardware selects one of them arbitrarily. A potential issue may arise when software polls from multiple sources to the same endpoint: after servicing the higher priority source, the hardware may repeatedly select the same lower priority source for access. That means other same-lower priority requests may be blocked for a long time, and in the worst case if there are dependencies between the polling sequences, the software may run into a livelock state.
This issue only affects certain interconnect where in one switch module there are at least three sources that can access the same target simultaneously. Also note that when all requests are at the same priority level, the issue does not apply.
When multiple sources are simultaneously polling from the same endpoint, and there is expected dependency based on the read data, ensure that all sources are sending the read commands at the same priority level. The source that breaks the dependency should be at equal or higher priority than other dependent sources.