SPRZ491D december 2020 – june 2023 DRA821U , DRA821U-Q1
PCIe: The SerDes PCIe Reference Clock Output can exceed the 5.0 GT/s Data Rate RMS jitter limit
When operating the SerDes PCIe Reference Clock in Output mode, the RMS jitter of the clock may exceed the PCIe specification limit for the 5.0 GT/s Data Rate.
Option 1:
Configure the Reference Clock output in Derived Refclk mode (as opposed to Received Refclk mode) and program the PLL configuration registers as follows:
- Set CMN_PDIAG_PLL0_CP_PADJ_M0 = 0x0128 to enable lower jitter operation
(Note for Devices that support 8.0 GT/s operation: Derived Refclk mode has an associated errata i2242 related to temporary disabling of the Refclk while changing Data Rates to/from 8.0 GT/s in a Single PLL SerDes Configuration).
Option 2:
Do not operate the PCIe interface at the 5.0 GT/s Data Rate.
Option 3:
Use an external clock source to supply the PCIe Reference Clock to both the Root Complex and End Point Devices of the Link.