SPRZ491D december 2020 – june 2023 DRA821U , DRA821U-Q1
DDR: Entry and exit to/from Deep Sleep low-power state can
cause PHY internal clock misalignment
When DDR PHY enters the Deep Sleep low-power state, there is a delay before the PHY PLL is disabled and gated off. If exit from Deep Sleep occurs before the PHY PLL is disabled, the PHY internal clocks can get misaligned with respect to each other, resulting in timing failures inside the PHY.
If using software-initiated low-power mode by writing to LP_CMD in the DENALI_CTL_132 register, ensure that when entry into low-power mode has been acknowledged, wait for a minimum of 160 DDR clock cycles before requesting an exit from low-power mode. Another option is to use the following workaround.
If using PSC to disable the DDR interface, ensure that after disabling of DDR interface has been acknowledged, wait for a minimum of 160 DDR clock cycles before sending a request to enable it. Another option is to use the following workaround.
If using the controller’s automatic mechanism for low power entry/exit using LP_AUTO_ENTRY_EN in the DENALI_CTL_141 register, use the following workaround.
Workaround: Ensure that DDR PHY does not enter Deep Sleep low-power state.
This can be ensured by programming the value of PHY_LP_WAKEUP[3:0] in the DENALI_PHY_1318 register is greater than the values of all the following thresholds in DDR controller registers.
LPI_CTRL_IDLE_WAKEUP_FN, LPI_PD_WAKEUP_FN, LPI_SR_SHORT_WAKEUP_FN, LPI_SR_LONG_WAKEUP_FN, LPI_SRPD_SHORT_WAKEUP_FN, LPI_SRPD_LONG_WAKEUP_FN, LPI_SR_LONG_MCCLK_GATE_WAKEUP_FN, LPI_SRPD_LONG_MCCLK_GATE_WAKEUP_FN, and LPI_TIMER_WAKEUP_FN
where FN = F0, F1, and F2 for different frequency set points.