SPRZ506D October 2022 – December 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
Revisions Affected: 0, A, B, C
If the user is enabling interrupts using the EINT instruction inside an interrupt service routine (ISR) in order to use the nesting feature, then the user must disable the interrupts before exiting the ISR. Failing to do so may cause undefined behavior of CPU execution.