SPRZ530C April   2022  – July 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1

 

  1.   1
  2. 1Modules Affected
  3. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  4. 3Silicon Revision 1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 1.0 Usage Notes
      1.      i2134
    2. 3.2 Silicon Revision 1.0 Advisories
      1.      i2049
      2.      i2062
      3.      i2063
      4.      i2064
      5.      i2065
      6.      i2079
      7.      i2091
      8.      i2097
      9.      i2103
      10.      i2120
      11.      i2134
      12.      i2137
      13.      i2146
      14.      i2157
      15.      i2159
      16.      i2160
      17.      i2161
      18.      i2163
      19.      i2166
      20.      i2177
      21.      i2189
      22.      i2190
      23.      i2196
      24.      i2197
      25.      i2205
      26.      i2215
      27.      i2216
      28.      i2219
      29.      i2232
      30.      i2234
      31.      i2235
      32.      i2237
      33.      i2242
      34.      i2243
      35.      i2244
      36.      i2249
      37.      i2253
      38.      i2271
      39.      i2272
      40.      i2278
      41.      i2279
      42.      i2283
      43.      i2307
      44.      i2308
      45.      i2310
      46.      i2311
      47.      i2312
      48.      i2313
      49.      i2316
      50.      i2320
      51.      i2326
      52.      i2329
      53.      i2351
      54.      i2362
      55.      i2366
      56.      i2371
      57.      i2372
      58.      i2378
      59.      i2381
      60.      i2383
      61.      i2399
      62.      i2401
      63.      i2409
      64.      i2414
      65.      i2419
      66.      i2422
      67.      i2435
      68.      i2437
  5.   Trademarks
  6.   Revision History

i2242

PCIe: The SerDes PCIe Reference Clock Output is temporarily disabled while changing Data Rates

Details

The SerDes PCIe Reference Clock Output will be temporarily disabled when changing Data Rates to or from 8.0 GT/s in Derived Refclk mode (as opposed to Received Refclk mode) and using a single SerDes PLL to generate the PCIe TX and RX clocks. This is due to the PLL reprogramming which must be performed when changing the data rate from 2.5 GT/s or 5.0 GT/s to 8.0 GT/s in this mode.

Some external PCIe components that are using the PCIe Reference Clock may not tolerate the disabling of the clock when changing data rates. However, the SerDes in this Device family does not have an issue accepting this Reference Clock behavior. This means that a link that connects the SerDes in one Device to the SerDes in a second Device will not have an issue when one Device generates the Reference Clock and the other Device receives the Reference Clock.

Workaround

Option 1:

Configure the SerDes to use one PLL to generate the clocks for 2.5 GT/s and 5.0 GT/s data rates, and a second PLL to generate the clocks for 8.0 GT/s data rate. This option imposes some limitations:

A) If Internal SSC mode is used, the two PLLs will not spread in sync with each other. This could result in up to 5000ppm difference between frequency of the two PLLs, and therefore between the TX and RX of the link partners. Because of this, Internal SSC mode is not recommended.

B) Protocols used simultaneously with PCIe on different Lanes of the SerDes must be compatible with sharing the PLL configuration of at least one of the two PLLs used for PCIe.

Option 2:

Use Received Refclk mode. Note that this mode is impacted by the separate Output Refclk jitter errata advisory (i2241)

Option 3:

Do not operate the PCIe interface at the 8.0 GT/s Data Rate

Option 4:

Use an external clock source to supply the PCIe Reference Clock to both the Root Complex and End Point Devices of the Link.