SPRZ569 November 2024 F29H850TU
Flash: Stand-alone CPU1/CPU3 Reset With Flash Prefetch Enabled May Cause NMI to CPU1/CPU3
0
If Flash prefetch is enabled, a stand-alone reset issued to CPU1 or CPU3 (for example, debug reset from CCS) may cause an NMI to the CPU because of an uncorrectable ECC error. Below are the sources for a stand-alone CPU reset.
CPU1:
CPU3:
Disable Flash prefetch (FRIx_INTF_CTRL.PREFETCH_EN = 0) before issuing a stand-alone reset to the CPU.
CPU1 → FRI1_INTF_CTRL.PREFETCH_EN = 0
CPU3 → FRI3_INTF_CTRL.PREFETCH_EN = 0