CONTROLSS |
i2352 — CONTROLSS-SDFM: Dynamically
Changing Threshold Settings (LLT, HLT), Filter Type, or COSR
Settings Will Trigger Spurious Comparator Events |
YES |
CONTROLSS |
i2353 — CONTROLSS-SDFM: Dynamically
Changing Data Filter Settings (Such as Filter Type or DOSR) Will
Trigger Spurious Data Acknowledge Events |
YES |
CONTROLSS |
i2354 — CONTROLSS-SDFM: Two Back-to-Back
Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN
Within Three SD-Modulator Clock Cycles can Corrupt SDFM State
Machine, Resulting in Spurious Comparator Events |
YES |
CONTROLSS |
i2356 — CONTROLSS-ADC: Interrupts may Stop
if INTxCONT (Continue-to-Interrupt Mode) is not Set |
YES |
CONTROLSS |
i2357 — CONTROLSS-ePWM: An ePWM Glitch can
Occur if a Trip Remains Active at the End of the Blanking
Window |
YES |
CONTROLSS |
i2358 — CONTROLSS-ePWM: Trip Events Will
Not be Filtered by the Blanking Window for the First 3 Cycles After
the Start of a Blanking |
YES |
CONTROLSS |
i2359 — CONTROLSS-CMPSS:Prescaler counter
behavior different from spec when DACSOURCE is made 0 or
reconfigured as 1 |
YES |
CONTROLSS |
i2405 — CONTROLSS: Race condition OUTPUT_XBAR and PWM_XBAR resulting in
event miss |
YES |
CPSW |
i2345 — CPSW: Ethernet Packet corruption
occurs if CPDMA fetches a packet which spans across memory
banks |
YES |
CPSW |
i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock |
YES |
CPSW |
i2438 — CPSW: Host to Ethernet Checksum Generation with VLAN
ADD/Remove |
YES |
CPSW |
i2439 — CPSW: Host to Ethernet Timestamp Accuracy Issue |
YES |
UART |
i2310 — USART: Erroneous triggering of
timeout interrupt |
YES |
UART |
i2311 USART Spurious DMA Interrupts — USART: Spurious DMA Interrupts |
YES |
M4 ROM |
i2403 — M4 ROM: SBL redundant boot image feature not supported on HSSE
devices |
YES |
MBOX |
i2404 — MBOX: Race condition in mailbox registers resulting in events
miss |
YES |
ROM |
i2426 — ROM does not support OSPI 8D boot mode for the flashes
supporting extended opcode |
YES |
RAM SEC |
i2427 — RAM SEC can cause Spurious RAM writes resulting in L2 &
MBOX memory corruption |
YES |
DTHE |
i2428 — AES in DTHE generates extra dma request for data_in at the end
of GCM encrypt |
YES |
SOC CONTROL |
i2394 — Race condition in interrupt and error aggregator capture
registers resulting in events miss |
YES |
SOC CONTROL |
i2392 — Race condition in mem-init capture registers resulting in
events miss |
YES |
BUS SAFETY |
i2393 — Granular error status not logged in BUS_SAFETY_ERR registers
for the detected faults |
YES |
OSPI |
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode |
YES |
OSPI |
i2351 — OSPI: Direct Access Controller (DAC) does not support
Continuous Read mode with NAND Flash |
YES |
OSPI |
i2189 — OSPI: Controller PHY Tuning Algorithm |
YES |
PBIST |
i2374 — PBIST: PBIST fails if clock frequency of R5SS_CORE_CLK is not
same as R5FSS_CLK_SELECTED frequency |
YES |
ICSS |
i2433 — ICSS: Reading the 64-bit IEP timer does not have a lock MSW
logic when LSW is read |
YES |