SPRZ575A March 2024 – April 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Table 1-1 shows the module(s) that are affected by each usage note.
MODULE | USAGE NOTE |
---|---|
USB | i2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation |
Table 1-2 shows the module(s) that are affected by each advisory.
MODULE | ADVISORY |
---|---|
BCDMA | i2431 — BCDMA: RX Channel can lockup in certain scenarios |
i2436 — BCDMA: BCDMA RX_IGNORE_LONG setting in RX CHAN CFG register doesn't work | |
Boot | i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation |
i2372 — Boot: ROM doesn't support select multi-plane addressing schemes in Serial NAND boot | |
i2410 — Boot: ROM may fail to boot due to i2409 | |
i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled | |
i2457 — Boot: Missing data in UART transfer causes boot failures | |
C7x SE | i2120 — C71x: SE Hangs on Non-Parity Error Detection in Transposed Streams With LEZR |
i2199 — C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary | |
i2399 — C7x: CPU NLC Module Not Clearing State on Interrupt | |
CPSW | i2208 — CPSW: ALE IET Express Packet Drops |
i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up | |
CSI | i2190 — CSI_RX_IF may enter unknown state following an incomplete frame |
DDR | i2160 — DDR: Valid VRef Range Must be Defined During LPDDR4 Command Bus Training |
i2330 — DDRSS Register Configuration Tool Updates | |
DSS | i2097 — DSS: Disabling a Layer Connected to Overlay May Result in Synclost During the Next Frame |
ECC AGGR | i2049 — ECC AGGR: Potential IP Clockstop/reset sequence hang due to pending ECC Aggregator interrupts |
IA | i2196 — IA: Potential deadlock scenarios in IA |
MCAN | i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID |
i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID | |
MMCSD | i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small |
i2478 — MMCSD0: HS400 Mode not supported | |
OSPI | i2189 — OSPI: Controller PHY Tuning Algorithm |
i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable | |
i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash | |
i2383 — OSPI: 2-byte address is not supported in PHY DDR mode | |
PCIe | i2242 — PCIe: The SerDes PCIe Reference Clock Output is temporarily disabled while changing Data Rates |
i2243 — PCIe: Timing requirement for disabling output refclk during L1.2 substate is not met | |
i2326 — PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits | |
PLL | i2424 — PLL: PLL Programming Sequence May Introduce PLL Instability |
PRG | i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure |
PSIL | i2137 — Clock stop operation can result in undefined behavior |
RAT | i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set |
Reset | i2407 — RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low |
SGMII | i2362 — 10-100M SGMII: Marvell PHY does not ignore the preamble byte resulting in link failure |
USART | i2310 — USART: Erroneous clear/trigger of timeout interrupt |
i2311 — USART: Spurious DMA Interrupts | |
USB | i2409 — USB2 PHY locks up due to short suspend |