SPRZ580 December   2024 AM62D-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2134
      4.      i2189
      5.      i2196
      6.      i2199
      7.      i2208
      8.      i2249
      9.      i2278
      10.      i2279
      11.      i2310
      12.      i2311
      13.      i2312
      14.      i2366
      15.      i2371
      16.      i2120
      17.      i2137
      18.      i2253
      19.      i2383
      20.      i2401
      21.      i2407
      22.      i2409
      23.      i2410
      24.      i2376
      25.      i2399
      26.      i2413
      27.      i2414
      28.      i2417
      29.      i2419
      30.      i2420
      31.      i2421
      32.      i2422
      33.      i2423
      34.      i2431
      35.      i2435
  4.   Trademarks
  5.   Revision History

i2196

IA: Potential deadlock scenarios in IA

Details:

The interrupt Aggregator (IA) has one main function, which is to convert events arriving on the Event Transport Lane (ETL) bus, can convert them to interrupt status bits which are used to generate level interrupts. The block that performed this function in IA version 1.0 was called the status event block.

In addition to the status event block, there are two other main processing blocks; the multicast event block, and the counted event block. The multicast block really functions as an event splitter. For every event it takes in, it can generate two output events. The counted event block is used to convert high frequency events into a readable count. It counts input events and generates output events on count transitions to/from 0 to/from non-zero count values. Unlike the status event block, the multicast and counted event blocks generate output ETL events that are then mapped to other processing blocks.

An issue was found after design that could cause the IA to deadlock. The issue occurs when event “loops” occur between these three processing blocks. It is possible to create a situation where a processing block can not output an event because the path is blocked, and since it can not output an event, it can not take any new input events. This inability to take input events prevents the output path from being able to unwind, and thus both paths remain blocked.

Workaround(s):

Figure 2-1 shows the conceptual block diagram of IA 1.0. Potential loops are avoided by adopting the policy of not allowing the counted event block to send events to the multicast block. This method was chosen because it is more common to split an event first, and then count one while sending the other elsewhere. With this path blocked by convention, it is not possible for a single event to visit any block more than once and thus not possible for paths to become blocked so long as the outputs remain unblocked.

 Interrupt Aggregator Version 1.0 Figure 2-1 Interrupt Aggregator Version 1.0

By following the conventions outlined here, the system is safe from looping hazards that can create a deadlock scenario.