SPRZ580 December   2024 AM62D-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2134
      4.      i2189
      5.      i2196
      6.      i2199
      7.      i2208
      8.      i2249
      9.      i2278
      10.      i2279
      11.      i2310
      12.      i2311
      13.      i2312
      14.      i2366
      15.      i2371
      16.      i2120
      17.      i2137
      18.      i2253
      19.      i2383
      20.      i2401
      21.      i2407
      22.      i2409
      23.      i2410
      24.      i2376
      25.      i2399
      26.      i2413
      27.      i2414
      28.      i2417
      29.      i2419
      30.      i2420
      31.      i2421
      32.      i2422
      33.      i2423
      34.      i2431
      35.      i2435
  4.   Trademarks
  5.   Revision History

i2351

OSPI: Direct Access Controller (DAC) does not support Continuous Read mode with NAND Flash

Details:

The OSPI Direct Access Controller (DAC) doesn’t support Continuous Read mode with NAND Flash since the OSPI controller can deassert the CSn signal (by design intent) to the Flash memory between internal DMA bus requests to the OSPI controller.

The issue occurs because “Continuous Read” mode offered by some OSPI/QSPI NAND Flash memories requires the Chip Select input to remain asserted for an entire burst transaction.

The SoC internal DMA controllers and other initiators are limited to 1023 B or smaller transactions, and arbitration/queuing can happen both inside of the various DMA controllers or in the interconnect between any DMA controller and the OSPI peripheral. This results in delays in bus requests to the OSPI controller that result in the external CSn signal being deasserted.

NOR Flash memories are not affected by CSn de-assertion and Continuous Read mode works as expected.

Workaround(s):

Software can use page/buffered read modes to access NAND flash.