SPRZ580 December 2024 AM62D-Q1
Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled
If PLL Deskew calibration is being disabled, the ROM driver code intends to check if deskew calibration is enabled and if lock has failed. However the current code has an assignment in an if condition. As a result, it does not check if deskew calibration is enabled before clearing the config bit. There is no functional issue.
None