Wenhao Wu
Lithium thionyl chloride (LiSOCI2) batteries are popular in smart flow meters because they provide higher energy density and a better cost-per-wattage ratio than battery chemistries such as lithium manganese dioxide (LiMnO2). One disadvantage of LiSOCl2 batteries is poor response to peak loads, which can result in a decrease of the usable battery capacity. So in this article, we’ll describe an effective method to decouple peak loads from the battery, in the range of a few hundred milliamperes, that can help increase battery life.
Maximizing the usable battery capacity is important because it enables the system design to support:
The overall effect minimizes battery and maintenance costs, as well as development costs, by enabling more reuse of a single flow meter design across more kinds of flow meters
Watch the TPS61094 in action | |
See how the TPS61094 buck/boost converter maintains ultra-low IQ while integrating supercapacitor charging support in our video "Achieve ultra-low 60-nA IQ with the TPS61094." |
A successful meter design needs to sustain a long operational time (>15 years) while enabling functionalities such as valve control, data recording and data transmission. Extending battery life is an effective way to increase meter operational time. If you connect the battery to the load directly without any power buffer in between, however, the meter’s complex load profile may deteriorate the battery’s lifetime performance.
Based on the current level, you can divide the load consumption profile of a standard meter into standby mode, middle-stage mode and active mode. Each mode influences battery life differently:
Table 1 demonstrates the Saft LS33600 battery’s capacity derating vs. nominal capacity of 17 Ah at different load and temperature conditions. At an operating temperature of +20°C, a 200-mA load current leads to a 42% capacity degradation. Therefore, the battery should never directly supply the load. Only by employing a low-leakage power buffer can you limit the peak current to less than 10 mA.
Capacity (Ah) | –40°C | –20°C | +20°C |
10 mA | –41.2% | –17.6% | No derating |
100 mA | –82.35% | –58.8% | –23.5% |
200 mA | N/A | N/A | –42.0% |
TI’s 60-nA IQ buck/boost converter, the TPS61094, helps extend battery life while maintaining excellent efficiency over standby, middle-stage and active modes. The TPS61094 has three main benefits:
The usable energy in the supercapacitor is defined by the capacity of the supercapacitor, the set maximum voltage across the supercapacitor and the undervoltage lockout of the TPS61094. The more usable energy that a supercapacitor has, the longer the operating time with a continuous, heavy load.
Figure 3 shows a power-buffer solution using the TPS61094 or only supercapacitors, respectively. For the TPS61094 solution, the supercapacitor voltage is set to 2 V. By supplying a continuous load, the TPS61094 can draw power from the supercapacitor until 0.6 V. Therefore, it is possible to calculate the available energy on the supercapacitor with Equation 1:
where ŋ is average efficiency of the converter.
In the worst case of –40°C, the TPS61094 has an average efficiency of 92% at 150 mA for an input voltage from 2 V to 0.6 V. Equation 2 shows the calculated result:
For HLC or EDLC solutions, the available energy changes following the battery voltage. For a 10-mA current at –40°C, the LS33600 voltage reduces to 3 V. Equation 3 calculates the available energy:
Comparing results between Figure 2 and Figure 3, the TPS61094 solution has double the available energy of the HLC and EDLC solutions. This means more energy can be delivered to loads, and lowers the peak current drawn from the battery under extreme conditions. For example, if there is a 200-mA load at 3.3 V to drive a valve, an HLC or EDLC solution can only support the load for 2.8 s. The TPS61094 buck/boost converter with an integrated supercapacitor can support the load for as long as 7.8 s, assuming that the power buffer supplies all of the load.
The complex load-consumption profile of flow meters requires a power buffer to help extend LiSOCl2 battery life. With excellent efficiency over wide operating conditions, the TPS61094 is a good choice to remove lifetime extension challenges. By limiting the peak current drawn from the battery, this buck/boost converter maximizes its capacity and raises the supercapacitor’s available energy, enabling the system to operate longer in low-temperature conditions than an HLC or EDLC solution.