Matt Hein
(This article was originally published on Planet Analog.)
Quick – what are the three motor types? The most common answer that I hear is "brushed-DC motors, stepper motors and brushless-DC motors," which is basically a knee-jerk reaction to the question. Some of the more intrepid motor-drive experts I know might say "single-phase AC input, multiphase AC input or DC input," categorizing each motor by its input mechanism rather than the specific motor type. I will admit, this is a pretty clever answer. There is certainly no shortage of different possible groupings in the taxonomy of motors, ranging from the use of position sensors to the supply voltage to the driver implementation; some engineers may be tempted to try to answer in these ways, even though the response doesn't always fit into three distinct categories. In this technical article, I'll address a new way to look at motor classification.
I have recently become fascinated with the idea that we should classify motors by their function. Many applications use different kinds of motors depending on the whim of the designer, but the same motor solution may not even be applicable in a different application that uses the same kind of motor. If that sentence gave you a headache (my communications colleague assured me that it had this effect on her), let me give you a better example: you can implement a pan-tilt-zoom (PTZ) camera axis with a stepper motor, a brushless-DC motor or even a brushed-DC motor. A brushless-DC motor is also the most common motor type in a ceiling fan (see Figure 1). But you can't use the same brushless-DC motor solution for both of these end-equipment types. A ceiling fan driver circuit, however excellent its performance, would be a horrible choice for a PTZ camera, and result in a product that just doesn't work. Why do I know this? Intuitively, I recognize (as you probably do as well) that the "function" of a ceiling fan motor and the "function" of a PTZ camera motor are very different, even though both are using a brushless-DC motor. There must be a property of motor functionality from an application perspective that can help establish a different classification of motor types.
So what are these motors actually doing? The function of a ceiling fan is to spin at a constant speed to circulate air in a room. The function of a PTZ camera is to move the camera to a certain position and hold it there. I can add a third example in to the mix – a cordless power drill. The user controls the drill's torque by pressing the trigger, perhaps to drill a bit through a wall stud. These motors have very distinct implementations; thus, my answer to "What are the three motor types?" is an emphatic "Speed, torque and position." Take a look at Figure 2 and Table 1 below.
Type | Example | Load | Top priority | Sensorless capability |
---|---|---|---|---|
Speed | Ceiling fan | Air or fluid | High speed and low noise | Easy |
Torque | Power drill | Solid | High power density | Very hard |
Position | PTZ camera | Solid | High accuracy and efficiency | Extremely hard(1) |
Let's talk more about speed, torque and position in the Understanding brushless-DC motor systems, part 2 technical article.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated