Shaury Anand
Test and measurement applications like battery test, electrochemical impedance spectroscopy and semiconductor test require accurate current- and voltage-output DC power supplies. The current and voltage control accuracy of the equipment need to be better than ±0.02% of the full-scale range over a ±5°C ambient temperature change. The accuracy largely depends on temperature drift of the current-sense resistor and amplifiers. In this article, you will learn how different components affect system accuracy, and how to choose suitable components for a precision DC power-supply design.
Figure 1 is a block diagram of a power supply, including an output driver, current- and voltage-sensing circuits, control loops, an analog-to-digital converter (ADC) and a digital-to-analog converter (DAC). The selection of an output driver depends on output accuracy, noise and power level. A linear power is used as an output driver for low-power (<5 W) or low-noise applications. A power operational amplifier (op amp) with integrated thermal and overcurrent protection is suitable for low-power applications.
Using a linear output driver for higher output power is challenging because of power dissipation, however, so you’ll need a synchronous buck converter for higher output power, which can achieve 0.01% of full-scale range accuracy by keeping big filters at the output. For example, a 5-V output range can achieve 500-µV accuracy using a buck converter. You’ll also need to confirm that there are no pulse-skip and diode emulation modes in the converter, which increase output ripple at light loads. The C2000™ real-time microcontroller (MCU) is a good fit for precision synchronous buck converter power supplies because you can disable features you don’t want in the software.
A high-precision current shunt resistor and a low-drift instrumentation amplifier can measure the output current. The instrumentation amplifier’s input offset error and gain error are not a concern, as both errors are accounted for during system calibration. The instrumentation amplifier’s offset and gain drift, output noise, and gain nonlinearity are difficult to calibrate, however, and you should consider these errors when selecting a current-sense amplifier.
Equation 1 calculates the total unadjusted error of the current-sense amplifiers shown in Figure 2. The error from the common-noise rejection ratio is relatively small, and you can ignore it.
The INA188 has the least error among the amplifiers listed in the table. The error calculations use a ±5°C temperature variation, with 100-mΩ and 1-mΩ current resistors chosen for 1-A and 25-A outputs, respectively.
Using a differential or instrumentation amplifier enables you to monitor the load voltage very accurately. The amplifier senses both loads’ output voltage and ground to eliminate error from any voltage drop in the cables. System calibration adjusts the offset and gain errors of the amplifier, leaving only input offset drift. You can calculate the drift in parts per million by dividing the offset drift by the full-scale voltage. For example, with a 2.5-V full-scale range and 1-µV/°C offset drift, the drift will be 0.4 ppm/°C. If you need a lower-output voltage drift, you can choose a zero-drift op amp such as the OPA188, which has a maximum input offset drift of 85 nV/°C. However, 1-µV/°C offset drift precision op amps are sufficient for most applications.
ADC offset and gain errors are adjusted during system calibration. Errors caused by drift and nonlinearity of the ADC are difficult to calibrate. Figure 3 compares errors of three different high-precision delta-sigma ADCs for a temperature variation ±5°C. The ADS131M02 has the least error among the ADCs listed in the table. The error calculation excludes the output noise of the ADC and the voltage reference error.
You can reduce error from noise significantly by increasing the oversampling ratio of the ADC. A low-noise (<0.23 ppmp-p) and low-drift voltage reference (<2ppm/°C) such as the REF70 is sufficient for DC power supply applications. The device has only 28 ppm of long-term drift for 0 to 1,000 hours of operation. The subsequent drift will be significantly lower than 28 ppm for the next 1,000 hours.
Figure 4 shows an analog control loop for the power supply. Even if you don’t need a constant-current output, keeping the constant-current loop will help with short-circuit protection. The constant-current loop will limit the output current by reducing the output voltage, and the current limit is programmable through the IREF setting.
Using a diode in between the constant-current and constant-voltage loops helps with constant voltage-to-constant current transition, or vice versa. A multiplexer-friendly op amp is suitable for constant-current and constant-voltage loops to avoid a short between amplifier inputs in open-loop operation. When any control loop is in an open-loop condition, the operational amplifier may see a differential voltage at its input pins greater than 0.7 V. A nonmultiplexer-friendly op amp has antiparallel diodes at the input pins, which doesn’t allow the differential voltage to exceed the diode drop. Therefore, a nonmultiplexer-friendly op amp increases the bias current of the amplifier, which may cause self-heating of the device and system inaccuracies as that current interacts with source impedances.
You can also implement control loops in digital domain inside C2000 real-time MCUs. High-resolution pulse-width modulation, a precision ADC and other analog peripherals of the C2000 real-time MCU help reduce the total number of components and bill of materials. The C2000 real-time MCU portfolio includes both 16- and 12-bit ADC options.
Consider temperature drift and noise specifications while designing a DC power supply for test and measurement applications. You can achieve less than 0.01% accuracy if you choose a low-drift amplifier and ADC products.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated