D. Harmon
Today’s vehicles have more intelligence and more connectivity than our mobile phones did 20 years ago. They are in near-constant communication with the world, whether through subscription-based communications services or built-in cellular functionality. In the future, this will include vehicle-to-vehicle communication. The core controlling communication to the outside world is the telematics control unit (TCU) (Figure 1).
In addition to the communication that happens when the vehicle is in motion, there is a need to communicate when the vehicle is turned off, for tasks like module firmware downloads, diagnostic uploads to cloud services or location services notifications.
For internal combustion engine-based vehicles, vehicle-off communication will always be a drain on the battery. While this might not be a concern for a charging electric vehicle, a noncharging electric vehicle runs into the same issue as an internal combustion vehicle. Although communication will not consume nearly enough power to drain a battery, if the vehicle is in an extended off-state (such as parked at the airport during a long trip), the drain does potentially become a concern. Therefore, it is important to understand how much power is being consumed by this vehicle off communication to ensure that there will be enough battery power left to start the vehicle when the owner returns. The current consumed is often referred to as “dark current.”
Different vehicles have different methodologies for monitoring their dark-current consumption. Many vehicles simply count the number of communication sequences that have occurred. When the count reaches a certain level, the TCU will slow down the frequency of communication and eventually stop it all together to preserve the battery’s state of charge. This method works well if all communications have equal power consumption.
If on the other hand, different communications consume different current amounts, it may be more beneficial to measure the actual consumption to better know the current being drained from the battery. Measuring this current presents two primary challenges:
TI’s INA186-Q1 addresses both challenges. The INA186-Q1 has a common-mode voltage range that extends up to 42 V, allowing it to survive on automotive 12-V battery rails. For more information on this topic, see the “12-V Battery Monitoring in an Automotive Module” application brief.
The ability to have a dynamic range of four decades of current measurement is a challenge for most current-sense amplifiers. For example, let’s say that you had these specifications:
Thus, you have an output voltage swing that is approximately half of the supply voltage (2.46 V – see section 7.4.3 of the INA186-Q1 data sheet for more information on bidirectional current measurement). To calculate the ideal shunt resistor value, you would want 10 A to be exactly 2.46 V. At a gain of 25, this translates to an input voltage of 98.4 mV. Therefore, the ideal shunt value is 9.84 mΩ. In reality, you will want to use a slightly lower-valued shunt resistor to ensure that you do not saturate the output over various operating conditions and shunt variations.
The root-sum-square method is used for error calculation. TI offers more on current measurement error calculation in our TI Precision Labs - Current Sense Amplifiers training series – specifically the TI Precision Labs - Current Sense Amplifiers: Introduction to Different Error Sources video. A first-order calculation using these four error sources – offset, gain error, common-mode rejection and power-supply rejection – results in the error levels shown in Table 1 at the two extreme currents.
Device | MaxVOUT (V) | Gain(V/V) | MaxVIN (V) | IdealRSHUNT (mΩ) | Errorat 0.01 A (%) | Errorat 10 A (%) |
---|---|---|---|---|---|---|
INA186A1-Q1 | 2.46 | 25 | 0.10 | 9.840 | 65.1% | 0.9% |
INA190A1-Q1 | 2.46 | 25 | 0.10 | 9.840 | 21.9% | 0.2% |
As you can see, the error at 10 mA is over 50%, which may be too high for the application. To improve the error at low currents, you’ll need an amplifier with better offset. The INA190-Q1 shown in Table 1 is a pin-for-pin upgrade to the INA186-Q1 that provides improved accuracy.
In addition, you need to comprehend the power dissipation of the system and the cost of the shunt resistor. At a maximum current of 10 A with a 9.84-mΩ shunt, the maximum power dissipation is just under 1 W. If you can tolerate the additional low-current error, it will likely be easier to identify a cost-effective 4.92-mΩ shunt with 0.5-W power dissipation than the original 9.84-mΩ shunt. The low-current error will increase, however, with half of the voltage drop at minimum current.
As vehicle-off communications increase, it is vital to ensure that the battery will retain enough charge to handle vehicle-start functions. Accurately measuring the current consumed is one way to help the vehicle manage this functionality. TI current-sense amplifiers can help solve challenges related to high-accuracy dark-current monitoring.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated