Heinz-Peter Beckemeyer
As we look ahead, it’s exciting to reflect on the last decade as being on the precipice of the biggest evolution in cars since their inception more than a century ago. As autonomous and electric vehicles continue to gain traction, cars in the next decade may look quite different from the cars of the 2010s.
Looking ahead, there are four high-level themes that will drive innovation in the automotive industry.
Digital cockpit
![]() |
Vehicle electrification
![]() |
Connected car![]() |
Autonomous driving![]() |
Enhancing the driving experience begins in the driver’s seat where the driver presides over a central command center, an integrated cockpit.
Government regulations worldwide are challenging automakers to reconfigure and reimagine the powertrain to reduce emissions. A glimpse ahead in 2019, we can categorize the trends into on a three-part spectrum.
Improving the overall efficiency of combustion engines. | Electrifying mechanical components to enable hybrids. | Designing fully electric vehicles. |
Within these categories, key trends have emerged:
Read the white paper and see the reference design: Bridging 12 V and 48 V in dual-battery automotive systems.
Encompassing more than fully self-driving cars, in 2019, autonomous driving in passenger vehicles will be experienced primarily through driver assistance functionality, features that are designed to mitigate or prevent human error on the road and improve the situational awareness of the driver.
Read the white paper to learn more: Paving the way to self-driving cars with advanced driver assistance systems.
Modern vehicles are as connected to the outside world as the driver is with their smartphone. Smart driving will become the norm with vehicles communicating with the driver, other cars on the road, infrastructure, the cloud and pedestrians—all while giving passengers the constant connection we’ve come to expect.
Learn more about telematics in the blog: Four design considerations for telematics hardware in the connected car.