SSZTA16 july   2019 ISO7731

 

  1.   1
  2.   2
    1.     3
    2.     Trends in Smart E-Meters
    3.     Additional Resources

Shashank Sharma and Vikas Kumar Thawani

All major countries are investing in the smart grid and are committed to making it a success. Why? Because power demand is going up, grid and power distribution will be critical. As demand increases, the cost of power increases because the resources to generate electricity are limited, resulting in huge growth in this segment). There are more than 900 million e-meters committed worldwide, with ~65% still to be deployed.

By definition, the smart grid means a bidirectional flow of energy and communication from generation to consumption (end to end). A smart meter is the key end equipment in this chain, which measures and sends power usage and supports automated billing, remote disconnection, time-of-use pricing models, and so on.

In this post, we will explain where you need isolation in a smart meter application.

Figure 1 shows an example smart meter, which includes a communication board that can have wired or wireless communication ports. The most commonly used wired communication interface used for meter-reading applications is RS-485. Here, isolation is required to break the ground potential difference between the energy meter and meter-reading node, which could be hundreds of meters away.

Certain e-meters have an RS-232 port to enable human operators to connect meter-reading equipment directly to the energy meter. In such cases, isolation is required to prevent electrical shock and any damage to meter-reading equipment from high-voltage surges that can appear on the AC mains.

GUID-0D83146D-EEC2-444F-BA05-90FFD397F04C-low.png Figure 1 Typical Block Diagram of Single Phase Smart E-Meter

In polyphase smart electricity, shunt sensors are becoming more popular than current transformers (CTs) for phase current sensing. The main benefit of using a shunt sensor over a CT is that the measurement function becomes more immune to magnetic tampering. Thus, the trend globally is toward shunt-based polyphase smart e-meters.

Figure 2 shows a system that needs to sample voltage and current for each phase. To preserve phase-to-phase isolation, you can use either a metrology microcontroller (MCU) or a dedicated analog-to-digital converter (ADC) for each phase. Grid parameters are sent across the isolation barrier to the host MCU, which performs data aggregation and communication. Thus, an isolation device is required between the host MCU and metrology MCUs/ADCs.

GUID-265B0825-60CA-4B54-930F-A106C7BED4D4-low.png Figure 2 Typical Block Diagram of Polyphase E-Meter

Another use case for isolation in smart electricity meters is when testing the e-meter’s active and reactive energy accuracy by connecting a reference meter. The smart e-meter outputs pulses at a rate proportional to the amount of energy consumed by the load. A reference meter determines the accuracy of the smart e-meter by calculating the error based on these pulses.

An isolation device provides galvanic isolation between the smart e-meter and the reference meter, as shown in Figure 3.

GUID-039A6A1A-6F2D-44DA-B930-808C9457B445-low.png Figure 3 Block Diagram Showing Energy Calibration in an E-Meter Design