SSZTAR1 october 2016 LM2902-Q1 , OPA365-Q1 , OPA4322-Q1 , TLC2272A-Q1 , TLV2372-Q1 , TPS92515HV-Q1 , TPS92661-Q1
Wen-Shin Wang
As a college student, I would often drive back to my dorm room very late at night. On my route, I would always have to drive on a long stretch of road with lots of overhanging trees on either side. It was beautiful by day but terrifying at night, as it seemed like other students would randomly pop out to walk right in front of my car.
Thankfully, my LED headlights were able to illuminate my fellow night owls. And behind the scenes, helping ensure that my headlights worked, was an often tiny but important device – the operational amplifier (op amp). In this blog post, I’ll cover the key parameters to consider when choosing an op amp for an external lighting application.
Before we drill down on the op amp, let’s summarize how LED lighting works. The current of the LED is the main consideration for lighting systems, as it controls the brightness and intensity of the light. The LED actually pulses a modulated light at above 200Hz – which the human eye averages out.
Because the LED current controls the brightness and intensity of the light, the op amp is often used as a current sense to help control the current going into the LEDs. High-current peaks in the pulse-width modulation (PWM) signal can overshoot the LED’s specified current level and negatively impact its life span. Figure 1 below shows the overall system block diagram of a LED headlight and where the op amp is used in the application.
To pick a suitable op amp as a current sense, it should have:
As cost is always a strong factor in these systems, TI offers a wide range of op amps suitable for external lighting applications, such as the TLC2272A-Q1 or TLV2372-Q1. For higher-resolution needs, the OPA365-Q1 is another option due to its wide bandwidth, very low offset and rail-to-rail output (RRO) features.
As the sun starts setting earlier, don’t forget about these op amps when you turn on your headlights and drive home into the night. See TI’s wide automotive op amp portfolio here, and visit TI’s body electronics and lighting overview page here for more information on system-level needs