• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Lighting the Road Ahead: LEDs in Automotive Front Lighting

    • SSZTAU1 september   2016 LM3423-Q1 , LM3424-Q1 , TPS92515HV-Q1 , TPS92661-Q1 , TPS92691-Q1

       

  • CONTENTS
  • SEARCH
  • Lighting the Road Ahead: LEDs in Automotive Front Lighting
  1.   1
  2.   2
    1.     3
    2.     Additional Resources
  3. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content
Technical Article

Lighting the Road Ahead: LEDs in Automotive Front Lighting

Issac Hsu

GUID-04F82147-F822-49CB-964D-DCDC3652215B-low.jpg

Light-emitting diodes (LEDs) are becoming more and more popular in automotive front lighting; for example, many cars on the road today use LEDs in daytime running lights (DRLs). Some high-end vehicles even have a full LED headlight or advanced matrix headlight installed. In this post, I will describe the most common automotive front-lighting architectures and some possible developments in this area.

Typical automotive front-lighting systems consist of a high-beam lamp, low-beam lamp, turn light, DRL and fog lamp. Except DRLs, most of these functions have traditionally used incandescent, Xenon or high-intensity discharge (HID) lamps. The simplest way to replace lamps with LEDs in headlights is to implement each function with an individual LED driver and connect a suitable number of high-brightness LEDs. Such an architecture, shown in Figure 1, is called a single-stage architecture, since a DC/DC LED driver, regulating a constant current, handles each individual lighting function.

GUID-C88FC87D-EB45-4925-A84F-E851A0E97332-low.png Figure 1 Single-stage Architecture for Automotive Front Lighting

In a single-stage architecture, the converter needs to handle wide input-voltage variations from the car battery at extreme conditions such as load dump, crank, etc. It is common to have either a boost or buck-boost conversion topology. While some carmakers would prefer to implement the position lamp function together with the DRLs, it is also desirable to implement a dimming function with the LED driver. There are different Automotive Electronics Council (AEC)-Q100-qualified low-side N-FET controller devices from TI which can nicely implement this type of LED driver, such as the TPS92691-Q1, LM3424-Q1 and LM3423-Q1.

The platform approach is a recent trend in how to implement a full LED headlight. As shown in Figure 2, an intermediate boost converter handles all car battery voltage variations and provides a high output voltage, such as 48 V, that can handle the various LED string lengths used for different headlight functions. As long as the LED string voltage is below 48 V, the DC/DC buck converters can act as LED drivers.

This platform approach could be called a two-stage architecture. The advantage of a two-stage architecture is that a boost converter handles the car battery’s input voltage variation, while buck LED drivers, which can be modularized, handling the individual headlight functions. TI recently released an AEC-Q100-qualified buck LED driver, the TPS92515HV-Q1, which can be used in a two-stage architecture.

GUID-82C3AA0F-8032-48BB-B7E3-A5AE415E1C2C-low.png Figure 2 Two-stage Architecture for Automotive Front Lighting

One of my previous blog posts described an adaptive headlight which could improve road safety. In the post, I introduced a matrix-manager device, the TPS92661-Q1. Let’s look at how to construct such a system from an automotive front-lighting perspective, regardless of the advanced driver-assistance system (ADAS) camera. The two-stage architecture is easily adoptable as an adaptive headlight by adding matrix-manager devices to individual LEDs according to different headlight functions, as shown in Figure 3.

GUID-D3583AA0-EBCB-456D-8966-84A3C5A07461-low.png Figure 3 Adaptive Headlight Based on a Two-stage Architecture with Matrix-manager Devices

The matrix-manager devices control individual LED brightness/on/off through a microcontroller unit (MCU) running on a digital protocol. This technique can realize different advanced lighting features, from a simple sequential turn or welcome light to a complicated anti-glaring function. Because an LED’s brightness/on/off changes dynamically according to road situations (analyzed by the ADAS system, not shown in Figure 3), the buck LED driver should be able to operate fast enough so there is no potential voltage/current overshoot event to damage the LEDs. Buck drivers such as TPS92515HV-Q1, which support shunt-FET dimming, would be the best choice for such a system.

Designing with LEDs can result in better automotive front-lighting systems. Vehicles on the road not only have gorgeous headlights, but headlights which can also enhance road safety. Get more information on a wide variety of automotive LED drivers from TI and follow “Behind the Wheel” for more blogs on automotive LED lighting and electronics.

Additional Resources

  • Read James Patterson’s Electronic Design article, “LED-Driver Electronics Enhance Headlight Style, Safety, and Reliability.”
  • Read other blogs on LED lighting.
  • Discover what’s new with Automotive LED drivers.
  • Watch an introduction to the TPS92661-Q1.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale