Maxim Altshul
Wireless audio appeared a few years ago, and has been progressing and improving since then. In recent years, manufacturers have turned to Wi-Fi® as a method to transfer audio data which makes a lot of sense for the following reasons:
Sounds perfect right?
Well, like any technology implementation there are challenges to overcome. Here, the problem starts with infrastructure. When using a standard star Wi-Fi topology, all speakers must be connected to a single central entity to play music, which limits the user in the placement of home speakers, for example.
The solution? IEEE 802.11s: Or in a less formal name – mesh. With a mesh topology, the possibilities grow larger and limitations dwindle. Infrastructure? No problem. With mesh, every node is connected to each other and everything is efficiently distributed across the network with no central entity. In essence, mesh allows devices with the same configured profile to connect to each other on MAC level. For example, two speakers that are not in range of each other can still be connected through other speakers between them that are in range, turning each speaker into a range extender, among other things.
Mesh packs a lot of features:
But the most important feature is this: 802.11s is a standard and we at TI have embraced it and now provide mesh capabilities on all of our WiLink™ 8 Wi-Fi + Bluetooth® modules.
Our WiLink 8 Wi-Fi mesh solutions offer even more features than standard implementations:
Imagine this: You go to the beach with your friends and each person brings their own wireless speaker. They all connect, sync flawlessly and play your music – together.
Want to get more oomph out of your sound system? Get another speaker and place it in the range of another and you are done! Have a set of speakers in your basement but no network coverage? Use mesh to extend your network’s range to turn your basement into a dance hall!
A Wi-Fi mesh system will allow a seamless connection that can cover your entire home, even when no central entity is present. Just place that speakers anywhere you want and get that music going!
The solutions and possibilities that a mesh system brings to wireless audio are endless, and with our WiLink 8 combo-connectivity modules you can start making your own today!
So, shall we Tango?