Rachel Liao
Capacitive sensing is an effective technique for applications ranging from proximity detection and gesture recognition to liquid level sensing. Depending on the application, there will be different system requirements regarding sensitivity, responsiveness and power. Power consumption is a key parameter for many applications, including wearables, consumer electronics and some automotive applications. So how do you reduce the power consumption of your system? In this post, I’ll describe techniques to reduce power consumption for capacitive-to-digital converters. I conducted various experiments to verify the effectiveness of these power-reducing techniques.
Capacitive sensing is currently using different circuit architectures, as I explained in my previous capacitive sensing architecture comparison blog post. In particular, the inductor-capacitor (LC) tank architecture measures the change in oscillation frequency to determine the change in capacitance. The tank oscillation frequency (fOSC) is compared to an independent reference clock (fREF) to produce an output sample that represents fOSC as a fraction of fREF. The power consumption of these types of devices is typically on the order of a few milliamps for continuous sampling modes. For low power applications, duty-cycling the device can help reduce the power consumption since the device is put into a lower-power mode and only active while it is performing a measurement conversion. This minimizes the total amount of current flowing through the device and therefore, reduces overall power consumption.
One of the main tradeoffs associated with this duty-cycling technique is responsiveness. The higher the sampling rate, the faster the system responsiveness is, but at the cost of higher average power. However, for applications that do not need an extraordinarily fast response time, a lower sampling rate can be used to achieve lower power consumption. For example, many human-machine interfaces (HMI) only need to run at sampling rates of 40 SPS or lower. The total conversion time of a measurement for a given sampling rate can also affect power consumption depending on the resolution requirements. This concept corresponds to the duty cycle of the device at a particular sampling rate.
A second important technique to reduce power consumption in these capacitive sensing devices is gating of the external reference clock. Simply put, the reference clock is also turned off whenever the device is put into a low power mode. This not only reduces the power consumed by the external clock, but also significantly reduces the leakage current from the device pins.
I tested these techniques using the TI Designs Noise-immune Capacitive Proximity Sensor System Reference Design, which uses a TI capacitive-sensing IC, the FDC2214. With only one channel (channel 0, proximity sensor) enabled, I measured the current flowing through the FDC2214 using a digital multi-meter. Figure 1 shows the test setup and the testing conditions are given in Table 1.
![]() |
The TIDA-00466 was programmed so that the FDC2214 was only operating in one of three states: active, sleep, and shutdown. For each state, the current consumption of the device was measured and given in Table 2.
![]() |
These supply current values are taken with a gated external reference clock. If the clock is not off while the FDC2214 is in sleep or shutdown mode, the power consumption in these modes will significantly increase as seen in Table 3. The clocking transitions result in an increase of the device input pin leakage currents, which is negligible when compared to the normal mode current, but is significant when added onto the lower power mode currents.
![]() |
Figure 2 shows an approximately linear relationship between current consumption and RCOUNT, as expected. Since RCOUNT is directly related to sensor conversion time, a lower RCOUNT results in a shorter conversion time and allows the device to spend less time actively running and more time in sleep mode (per sampling period). For a given sampling rate, a lower RCOUNT consumes less current, while a higher RCOUNT consumes more current. Another way to understand the relationship is that if RCOUNT is kept constant but the sampling rate is varied, the FDC2214 sampling at a higher rate consumes more power than a FDC2214 sampling at a lower rate.
Duty-cycling and clock-gating are effective techniques to minimize power consumption. To ensure minimal current flow through the device, turn off the external oscillator used as the reference clock while the device is in its lower-power mode. The resulting current values for varying RCOUNT values at different sampling rates follow expected trends. Also, the FDC211x/FDC221x Current Consumption Estimator provided by TI can be used as a reference tool for estimating a worst-case power consumption scenario.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated