Jean Picard
Power over Ethernet (PoE) offers a convenient approach to deliver electrical power through Ethernet cables, eliminating the need for other external power sources and separate power cabling for equipment connected in an Ethernet network.
One limitation of the current IEEE802.3at standard is that the powered device (PoE PD) is not allowed to consume more than 25.5W. Another is that power can be delivered only over two pairs, which results in cable loss and low overall system efficiency. As a result, many applications have so far been out of reach for PoE, including the lighting market.
However, once released, the IEEE802.3bt standard will be able to fix these shortcomings, while adding many more features that will enable the use of PoE for LED lighting applications.
Let’s first review why you should consider PoE for LED lighting applications:
Troffers, downlights and many others.
Now, let me give you some details on the IEEE802.3bt standard. As an active member of this committee, I can give you a short summary of the major changes from the current standard that will directly impact PoE lighting.
A first change concerns the maximum power that the load can consume. To address this, the committee created two new types, type 3 and type 4, to allow the PSE to source up to 60W and 90W (52V-57V), respectively. Combining these new types with power delivery over four pairs will result in even more power available at the PD end of the cable.The committee is also introducing a new concept called “extended power.”
An issue with the current standard is that the allocated PD input power is based on a worst-case maximum cable length, which is 100 meters. See Figure 1 below. The extended power concept solves this by allowing the PD to go beyond this limit, as long as it does not cause the PSE to source more than it allocated. This implies that the PD “knows” the cable resistance. System architectures where the Ethernet cables are very short can take advantage of this feature.
A second change to the standard is about the standby power, which is related to the power signature that a PD must generate in order to maintain the PSE power. The maintain power signature (MPS) consists of a specific DC current amplitude, time duration and duty cycle. The big change with the next standard is about reducing the time duration and duty cycle considerably, which will dramatically reduce the average standby power, while the lights are off and data communication remains active. See Figure 2.
A third change to the standard is about ensuring that lighting remains operational (or can quickly turn back on) independent of data communication. This results in more reliable operation. To achieve this, the committee has defined a new requirement for type 3 and type 4 PSEs to support the physical layer classification for any power level the PSE can support.
Fourth, the Autoclass feature will allow better power optimization by the PSE. Basically, it allows the PSE to set the power budget to the maximum PoE PD power through a power measurement, including the cable losses.
I’m seeking feedback from lighting industry leaders, system integrators, LED ballast manufacturers and potential PSE lighting switch manufacturers (endspan and midspans).
What do you think? Do any of the new features mentioned above pique your interest and why? Please comment below to share your thoughts.
Additional resources about:
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated