SSZTC54 september 2015
Most industrial equipment requires some method for a technician to interface with the equipment in order to capture diagnostic data or send configuration data to the machine. This can vary from things like water and electricity meters to manufacturing equipment. The interface to such a device should be secure, robust and have appropriate data throughput without adding too much additional cost or power.
Near Field Communication (NFC) is a great way to provide such a wireless service interface. NFC is a short range (typically <10cm) wireless communication protocol which operates using 13.56MHz in the magnetic field. The technology is proximity based, so there is no pairing procedure required before communication, easing the user experience. In its most basic form, the user will simply “tap” an NFC reader to the NFC tag to read some data. Use of the magnetic field allows for a very controlled communication range, which provides some inherent security. Encryption can also be utilized to increase the level of security. In addition to the security aspect, NFC is a good solution due to the standardization and adoption of the technology in smartphones and tablets. The first major smartphone including NFC was introduced in 2010. Since then, the adoption has grown quickly and five years later, most smartphones include this technology. The implementation of this technology can offer a very low-power or even no-power source when the device can harvest energy from the RF field.
Below are some of the identified use cases of NFC in service interface applications. Since this is still a fairly new technology and application, I expect to see additional use cases identified in the future.
In regards to device selection, the different use cases and requirements could warrant different classes of devices. A dynamic tag, such as RF430CL33xH, could be useful in diagnostics and configuration where access control and firmware updates would lean towards a full transceiver solution for additional operation modes and increased throughput, such as TRF79xxA.
I hope this provided some useful insight into the new use cases for NFC. Until next time, this is Eddie “tapping” out.