SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The procedure takes the following input parameter:
The procedure returns the following:
The procedure returns with error if the specified queue is empty, or if the first entry of the queue is already busy. Otherwise, the following is done:
Set pQueue->pCurrEntry->status = Busy
Set pEntry = pQueue->pCurrEntry