SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Recharge of VDDR can occur when the Sensor Controller requests low-power or power-down operational modes. A recharge causes VDDS current spikes that may affect AUX measurements. The Sensor Controller must follow the routine shown in Figure 20-10 to avoid power noise caused by VDDR recharge during a sensitive measurement.
The routine is only valid when AON_PMCTL:RECHARGECFG.MODE is set to COMPARATOR, as this setting allows the Sensor Controller to execute tasks in Low-Power or Power-Down operational modes.
The Sensor Controller can also detect if the system power controller recharges VDDR within a certain time interval. The procedure is described in AUX_SYSIF:RECHARGEDET (see Section 20.8.9).