SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Several parameters that are not configurable through the parameter structures can still be overridden by using the CMD_BLE5_RADIO_SETUP, CMD_RADIO_SETUP, CMD_UPDATE_RADIO_SETUP, or CMD_WRITE_FWPAR commands.
The parameters that can be overridden in Bluetooth low energy mode are described in the Bluetooth Specification documents listed in Related Documentation. The parameters can, for example, be used to improve performance or to create noncompliant behavior that may be useful in some cases. Examples follow: