SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
The procedure takes the following input parameter:
The procedure returns the following:
The procedure returns with error if the specified queue is empty. Otherwise, the following is done:
Set pQueue->pCurrEntry->status = Active