SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
The programmable current output connects to the positive input of COMPA, which makes it possible to charge an external capacitance connected to an analog-capable AUX I/O. Physically, this output also connects to the reference DAC output. This connection is not intended for ISRC usage. Hence, the connection shows as a dotted line in Figure 20-20.
When ISRC is enabled, it drives the current configured by ADI_4_AUX:ISRC.TRIM onto the COMPA_IN analog node or to ground. The connection controlled by AUX_ANAIF:ISRCCTL.RESET_N.
The user must ensure that the COMPA positive input only has one driver at all times. To avoid shorting signals together internally, TI provides ROM-based TI-DriverLib functions that ensure a break-before-make switching of the internal muxes.