SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
A RTC capture event can be set up on channel 1 by configuring a capture source in AON_EVENT:RTCSEL and setting channel 1 to capture mode in AON_RTC:CHCTL. The captured RTC value is available in the register AON_RTC:CH1CAPT after a capture event
Compare events are configured by writing to the corresponding channel compare register AON_RTC:CHnCMP.
If a compare value is set so that the compare value minus current value is larger than the seconds wrap-around time minus one second ( 232 × SCLK_LFperiod – 1), an immediate compare event is set to avoid losing the event.