SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
Automatic phase transition requires that the setup phase needs less than 17 sample clock periods to charge the S-H capacitor to the target voltage. This is generally not the case when the Reference DAC drives an external load.
Configure the automatic phase control with the sequence as follows:
The transition sets the AUX_EVCTL:EVSTAT3.AUX_DAC_HOLD_ACTIVE event.