SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The AUX Timer0 and Timer1 (AUX_TIMER01) peripherals are two identical 16-bit compare timers. The Sensor Controller is the primary owner of these peripherals. However, Timer01 ownership can be shared with or owned by the System CPU.
Timer01 peripheral features are:
The main purpose of the timers is to generate events for the AUX domain event bus subscribers. The timers are not used directly for waveform generation. Figure 20-23 shows the block diagram for a single timer.