SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The following configuration is required to measure the frequency of an event source waveform. Use the sequence that follows:
Figure 20-17 shows a generic event source waveform.
The TDC measures correct signal frequency if the selected event source waveform matches the requirements listed in Table 20-25.
Description | Label | Requirement |
---|---|---|
Minimum low time | t_minL | 208 ns |
Minimum high time | t_minH | 208 ns |
Minimum period | t_min | 416 ns |
If an event waveform does not directly fulfill these requirements, the user must complete the following sequence:
Fore more details, see Section 20.4.5.2.6.