SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
Timer2 has four event outputs:
The user can set and clear events manually by writing AUX_TIMER2:EVCTL. Manual update of an event output takes priority over automatic channel updates of the same event. Listed in decreasing order of priority, each event output can:
The event output is high for two counter clock periods, then goes low.
An event output may receive update requests from several channels at the same time. In this case, the event output is updated according to the previously stated priority list.