SWCU193A April 2023 – August 2024 CC2340R2 , CC2340R5 , CC2340R5-Q1
Table 15-7 lists the memory-mapped registers for the DMA registers. All register offset addresses not listed in Table 15-7 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Section |
---|---|---|---|
0h | STATUS | Status Register. | Go |
4h | CFG | Configuration Register. | Go |
8h | CTRL | Channel Control Data Base Pointer Register. | Go |
Ch | ALTCTRL | Channel Alternate Control Data Base Pointer Register. | Go |
10h | WAITONREQ | Channel Wait On Request Status Register. | Go |
14h | SOFTREQ | Channel Software Request Register. | Go |
18h | SETBURST | Channel Set UseBurst Register. | Go |
1Ch | CLEARBURST | Channel Clear UseBurst Register. | Go |
20h | SETREQMASK | Channel Set Request Mask Register. | Go |
24h | CLEARREQMASK | Clear Channel Request Mask Register. | Go |
28h | SETCHANNELEN | Set Channel Enable Register. | Go |
2Ch | CLEARCHANNELEN | Clear Channel Enable Register. | Go |
30h | SETCHNLPRIALT | Channel Set Primary-Alternate Register. | Go |
34h | CLEARCHNLPRIALT | Channel Clear Primary-Alternate Register. | Go |
38h | SETCHNLPRIORITY | Set Channel Priority Register. | Go |
3Ch | CLEARCHNLPRIORITY | Clear Channel Priority Register. | Go |
4Ch | ERROR | Error Status and Clear Register. | Go |
504h | REQDONE | Channel Request Done Register. | Go |
520h | DONEMASK | Channel Request Done Mask Register. | Go |
Complex bit access types are encoded to fit into small table cells. Table 15-8 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
Reset or Default Value | ||
-n | Value after reset or the default value |
STATUS is shown in Table 15-9.
Return to the Summary Table.
Status Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | TEST | R | 0h | 0x0: Controller does not include the integration test logic 0x1: Controller includes the integration test logic 0x2: Undefined ... 0xF: Undefined |
27-21 | RESERVED | R | 0h | Reserved |
20-16 | TOTALCHANNELS | R | 7h | Register value returns number of available uDMA channels minus one. For example a read out value of: 0x00: Show that the controller is configured to use 1 uDMA channel 0x01: Shows that the controller is configured to use 2 uDMA channels ... 0x1F: Shows that the controller is configured to use 32 uDMA channels (32-1=31=0x1F) |
15-8 | RESERVED | R | 0h | Reserved |
7-4 | STATE | R | 0h | Current state of the control state machine. State can be one of the following: 0x0: Idle 0x1: Reading channel controller data 0x2: Reading source data end pointer 0x3: Reading destination data end pointer 0x4: Reading source data 0x5: Writing destination data 0x6: Waiting for uDMA request to clear 0x7: Writing channel controller data 0x8: Stalled 0x9: Done 0xA: Peripheral scatter-gather transition 0xB: Undefined ... 0xF: Undefined. |
3-1 | RESERVED | R | 0h | Reserved |
0 | MASTERENABLE | R | 0h | Shows the enable status of the controller as configured by CFG.MASTERENABLE:
0h = Controller is disabled 1h = Controller is enabled |
CFG is shown in Table 15-10.
Return to the Summary Table.
Configuration Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | W | 0h | Reserved |
7-5 | PRTOCTRL | W | 0h | Sets the AHB-Lite bus protocol protection state by controlling the AHB signal HProt[3:1] as follows: Bit [7] Controls HProt[3] to indicate if a cacheable access is occurring. Bit [6] Controls HProt[2] to indicate if a bufferable access is occurring. Bit [5] Controls HProt[1] to indicate if a privileged access is occurring. When bit [n] = 1 then the corresponding HProt bit is high. When bit [n] = 0 then the corresponding HProt bit is low. This field controls HProt[3:1] signal for all transactions initiated by uDMA except two transactions below: - the read from the address indicated by source address pointer - the write to the address indicated by destination address pointer HProt[3:1] for these two exceptions can be controlled by dedicated fields in the channel configutation descriptor. |
4-1 | RESERVED | W | 0h | Reserved |
0 | MASTERENABLE | W | 0h | Enables the controller.
0h = Disables the controller 1h = Enables the controller |
CTRL is shown in Table 15-11.
Return to the Summary Table.
Channel Control Data Base Pointer Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | BASEPTR | R/W | 0h | This register point to the base address for the primary data structures of each uDMA channel. This is not stored in module, but in system memory, thus space must be allocated for this usage when uDMA is in usage |
7-0 | RESERVED | R | 0h | Reserved |
ALTCTRL is shown in Table 15-12.
Return to the Summary Table.
Channel Alternate Control Data Base Pointer Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | BASEPTR | R | 80h | This register shows the base address for the alternate data structures and is calculated by module, thus read only |
WAITONREQ is shown in Table 15-13.
Return to the Summary Table.
Channel Wait On Request Status Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLSTATUS | R | FFh | Channel wait on request status: Bit [Ch] = 0: Once uDMA receives a single or burst request on channel Ch, this channel may come out of active state even if request is still present. Bit [Ch] = 1: Once uDMA receives a single or burst request on channel Ch, it keeps channel Ch in active state until the requests are deasserted. This handshake is necessary for channels where the requester is in an asynchronous domain or can run at slower clock speed than uDMA |
SOFTREQ is shown in Table 15-14.
Return to the Summary Table.
Channel Software Request Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Set the appropriate bit to generate a software uDMA request on the corresponding uDMA channel Bit [Ch] = 0: Does not create a uDMA request for channel Ch Bit [Ch] = 1: Creates a uDMA request for channel Ch Writing to a bit where a uDMA channel is not implemented does not create a uDMA request for that channel |
SETBURST is shown in Table 15-15.
Return to the Summary Table.
Channel Set UseBurst Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Returns the useburst status, or disables individual channels from generating single uDMA requests. The value R is the arbitration rate and stored in the controller data structure. Read as: Bit [Ch] = 0: uDMA channel Ch responds to both burst and single requests on channel Ch. The controller performs 2R, or single, bus transfers. Bit [Ch] = 1: uDMA channel Ch does not respond to single transfer requests. The controller only responds to burst transfer requests and performs 2R transfers. Write as: Bit [Ch] = 0: No effect. Use the CLEARBURST.CHNLS to set bit [Ch] to 0. Bit [Ch] = 1: Disables single transfer requests on channel Ch. The controller performs 2R transfers for burst requests. Writing to a bit where a uDMA channel is not implemented has no effect |
CLEARBURST is shown in Table 15-16.
Return to the Summary Table.
Channel Clear UseBurst Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Set the appropriate bit to enable single transfer requests. Write as: Bit [Ch] = 0: No effect. Use the SETBURST.CHNLS to disable single transfer requests. Bit [Ch] = 1: Enables single transfer requests on channel Ch. Writing to a bit where a uDMA channel is not implemented has no effect. |
SETREQMASK is shown in Table 15-17.
Return to the Summary Table.
Channel Set Request Mask Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Returns the burst and single request mask status, or disables the corresponding channel from generating uDMA requests. Read as: Bit [Ch] = 0: External requests are enabled for channel Ch. Bit [Ch] = 1: External requests are disabled for channel Ch. Write as: Bit [Ch] = 0: No effect. Use the CLEARREQMASK.CHNLS to enable uDMA requests. Bit [Ch] = 1: Disables uDMA burst request channel [Ch] and uDMA single request channel [Ch] input from generating uDMA requests. Writing to a bit where a uDMA channel is not implemented has no effect |
CLEARREQMASK is shown in Table 15-18.
Return to the Summary Table.
Clear Channel Request Mask Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Set the appropriate bit to enable uDMA request for the channel. Write as: Bit [Ch] = 0: No effect. Use the SETREQMASK.CHNLS to disable channel Ch from generating requests. Bit [Ch] = 1: Enables channel [Ch] to generate uDMA requests. Writing to a bit where a uDMA channel is not implemented has no effect. |
SETCHANNELEN is shown in Table 15-19.
Return to the Summary Table.
Set Channel Enable Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Returns the enable status of the channels, or enable the corresponding channels. Read as: Bit [Ch] = 0: Channel Ch is disabled. Bit [Ch] = 1: Channel Ch is enabled. Write as: Bit [Ch] = 0: No effect. Use the CLEARCHANNELEN.CHNLS to disable a channel Bit [Ch] = 1: Enables channel Ch Writing to a bit where a uDMA channel is not implemented has no effect |
CLEARCHANNELEN is shown in Table 15-20.
Return to the Summary Table.
Clear Channel Enable Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Set the appropriate bit to disable the corresponding uDMA channel. Write as: Bit [Ch] = 0: No effect. Use the SETCHANNELEN.CHNLS to enable uDMA channels. Bit [Ch] = 1: Disables channel Ch Writing to a bit where a uDMA channel is not implemented has no effect |
SETCHNLPRIALT is shown in Table 15-21.
Return to the Summary Table.
Channel Set Primary-Alternate Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Returns the channel control data structure status, or selects the alternate data structure for the corresponding uDMA channel. Read as: Bit [Ch] = 0: uDMA channel Ch is using the primary data structure. Bit [Ch] = 1: uDMA channel Ch is using the alternate data structure. Write as: Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIALT.CHNLS to disable a channel Bit [Ch] = 1: Selects the alternate data structure for channel Ch Writing to a bit where a uDMA channel is not implemented has no effect |
CLEARCHNLPRIALT is shown in Table 15-22.
Return to the Summary Table.
Channel Clear Primary-Alternate Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Clears the appropriate bit to select the primary data structure for the corresponding uDMA channel. Write as: Bit [Ch] = 0: No effect. Use the SETCHNLPRIALT.CHNLS to select the alternate data structure. Bit [Ch] = 1: Selects the primary data structure for channel Ch. Writing to a bit where a uDMA channel is not implemented has no effect |
SETCHNLPRIORITY is shown in Table 15-23.
Return to the Summary Table.
Set Channel Priority Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Returns the channel priority mask status, or sets the channel priority to high. Read as: Bit [Ch] = 0: uDMA channel Ch is using the default priority level. Bit [Ch] = 1: uDMA channel Ch is using a high priority level. Write as: Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIORITY.CHNLS to set channel Ch to the default priority level. Bit [Ch] = 1: Channel Ch uses the high priority level. Writing to a bit where a uDMA channel is not implemented has no effect |
CLEARCHNLPRIORITY is shown in Table 15-24.
Return to the Summary Table.
Clear Channel Priority Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | W | 0h | Clear the appropriate bit to select the default priority level for the specified uDMA channel. Write as: Bit [Ch] = 0: No effect. Use the SETCHNLPRIORITY.CHNLS to set channel Ch to the high priority level. Bit [Ch] = 1: Channel Ch uses the default priority level. Writing to a bit where a uDMA channel is not implemented has no effect |
ERROR is shown in Table 15-25.
Return to the Summary Table.
Error Status and Clear Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-1 | RESERVED | R | 0h | Reserved |
0 | STATUS | R/W | 0h | Returns the status of bus error flag in uDMA, or clears this bit Read as: 0: No bus error detected 1: Bus error detected Write as: 0: No effect, status of bus error flag is unchanged. 1: Clears the bus error flag. |
REQDONE is shown in Table 15-26.
Return to the Summary Table.
Channel Request Done Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Reflects the uDMA done status for the given channel, channel [Ch]. It's a sticky done bit. Unless cleared by writing a 1, it holds the value of 1. Read as: Bit [Ch] = 0: Request has not completed for channel Ch Bit [Ch] = 1: Request has completed for the channel Ch Writing a 1 to individual bits would clear the corresponding bit. Write as: Bit [Ch] = 0: No effect. Bit [Ch] = 1: The corresponding [Ch] bit is cleared and is set to 0 |
DONEMASK is shown in Table 15-27.
Return to the Summary Table.
Channel Request Done Mask Register.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CHNLS | R/W | 0h | Controls the propagation of the uDMA done and active state to the assigned peripheral. Specifically used for software channels. Read as: Bit [Ch] = 0: uDMA done and active state for channel Ch is not blocked from reaching to the peripherals. Note that the uDMA done state for channel [Ch] is blocked from contributing to generation of combined uDMA done signal Bit [Ch] = 1: uDMA done and active state for channel Ch is blocked from reaching to the peripherals. Note that the uDMA done state for channel [Ch] is not blocked from contributing to generation of combined uDMA done signal Write as: Bit [Ch] = 0: Allows uDMA done and active state to propagate to the peripherals. Note that this disables uDMA done state for channel [Ch] from contributing to generation of combined uDMA done signal Bit [Ch] = 1: Blocks uDMA done and active state to propagate to the peripherals. Note that this enables uDMA done for channel [Ch] to contribute to generation of combined uDMA done signal. |