SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
The COMMAND_RESET command tells the bootloader to perform a system reset. Use this command after downloading a new Flash image to the CC13x4x10 and CC26x4x10 devices to cause the new application to start from a reset. The normal boot sequence occurs and the Flash image runs similarly as if a hardware reset had occurred. Also, use this command to reset the bootloader if a critical error occurs and the host device wants to restart communication with the bootloader.
The bootloader responds with an ACK signal to the host device before actually executing the system reset. This ACK signal informs the host that the command was received successfully, and the CC13x4x10 and CC26x4x10 devices are then reset.
The format of the packet including the command ID is as follows:
unsigned char ucPacket[3];
ucPacket[0] = <size=3>;
ucPacket[1] = <checksum>;
ucPacket[2] = COMMAND_RESET;